University

Hackster.io projects using Texas Instruments parts

Notice: The projects below are hosted by Hackster.io and posted by the Hackster community. By clicking on a project, you will be leaving Texas Instruments’ website.

Student projects

Home
Peltier Cooler

Mini-cooler powered by the Peltier module, designed for temperature setpoint control.

Likes : 4    Views : 1017
Humanoid Robot

Humanoid Robot designed to walk like human beings with the potential of acting as workforce in different application areas.

Likes : 13    Views : 1015
DIY Precision Foam Cutter!

Need to make a a small boat hull or shaped foam insulated enclosure? Let's heat up some wire and get to work with CNC precision.

Likes : 2    Views : 963
Node-Red-Mam

Visualize the IOTA-MAM upload and download data streams of your sensors using node-red!

Likes : 5    Views : 939
Basketball Counting Machine

To design a basketball net which is able to count the number of successful baskets done by the player each time he/she throws the ball.

Likes : 7    Views : 925
Automotive Sensor Fusion Collision Avoidance System

Designed and built an autonomous braking collision avoidance system for a remote control car using Sonar and LiDAR sensors.

Likes : 2    Views : 925
Line Following Robot

This robot follows a dedicated path and can prove to be extremely useful in warehouse management, hotel industry and medical domain

Likes : 5    Views : 919
ECE434 Beaglebone BoneBot

This project is a wireless drone that can be controlled using the Blynk app on your phone. It has an autonomous mode that avoids objects.

Likes : 3    Views : 910
UARK Senior Design Project: BLDC Motor Controller

This project consists of designing a motor controller that will operate a 48V, 1hp BLDC hub motor.

Likes : 4    Views : 889
Wood Gas Generator (Energy From Waste)

Generation of wood gas (fuel) using waste around us.

Likes : 32    Views : 881
Controlling Hardware with your Voice: Language Processing

Processing language is hard. Fortunately, it can be offloaded to giants such as Google, Amazon, Microsoft, or IBM. Welcome to the cloud.

Likes : 3    Views : 859
Photosynthesis Detection System

Save the Earth with this light detector which measures and displays the light intensity in an environment.

Likes : 4    Views : 846
Super Smash Blows

Playing with toy cars and buttons has never been so fun!

Likes : 5    Views : 839
Tonewheel Synthesizer

Inspired by the Hammond Organ, this device generates sound with custom tonewheels made using easy to find parts and a simple control scheme.

Likes : 2    Views : 837
IoT Pocket Gateway

Low-cost IoT Gateway made with open-source software and hardware. Software includes temperature, humidity, and ambient light sensing.

Likes : 1    Views : 816
Smart LPG Cylinder Stand

Take the worries of booking gas cylinder away use our innovative cylinder stand.

Likes : 6    Views : 812
Ball Beam Balance

The goal for this project is to control the position of a ball on a beam that is actuated by a motor while using 5 LED lights as indicator.

Likes : 2    Views : 810
Two-in-One Radar System

This system can be used as both a backup radar and a collision warning system.

Likes : 2    Views : 806
IoT-Based Socket Board

A portable socket board is designed that can be controlled through internet. It provides portable automation solution of devices with ease.

Likes : 7    Views : 778
Button Mashing Counter

Have your friends ever gotten mad and accused you for button mashing at Super Smash Bros? Well now your name is cleared!

Likes : 2    Views : 757
MSP432P401R Driver for Pixy2

This is a driver with user-friendly functions that provides interface between the Pixy2 and the MSP432P401R microcontroller.

Likes : 5    Views : 756
IoT-Based Robot with Temperature Notification System

We can send this robot to remote places where humans cannot reach, and can also get the temperature of that place.

Likes : 1    Views : 752
UW-Makeathon: Printed Circuit Car

This project merges the electrical control board and chassis of an RC car into one!

Likes : 4    Views : 748
Motion Sensor Based Device Control

Optimize the energy consumption by activating your appliances only when human being are present in a room.

Likes : 7    Views : 737