University

Hackster.io projects using Texas Instruments parts

Notice: The projects below are hosted by Hackster.io and posted by the Hackster community. By clicking on a project, you will be leaving Texas Instruments’ website.

LaunchPad Development Kit

Home
Juan Says: A Juanderful Memory Game

LED matching sequence game to test your memory; reach the end and brag your status as Juan of the Juanderful Few!

Likes : 6    Views : 182
RGB LED Selector

Not sure what colored light best sets the mood? Use the RGB LED to test every color of the visible light spectrum!

Likes : 4    Views : 180
Using YDLIDAR with TI TMS320F28379D

This is a tutorial on using TI TMS320F28379D launchpad to read YDLIDAR X2 data.

Likes : 2    Views : 178
UIUC ME 461 Final Project: BeerBot 1000

A robo-butler that fetches beer. Need I say more?

Likes : 2    Views : 174
UIUC ME 461 robot car project Haolin Zhang

Obstacles avoding robot car with the MPU 9250 used as the compass and the tera term will print the x, y coordinates of the car.

Likes : 1    Views : 160
Low Frequency Tracking SegBot - UIUC ME461

Your SegBot uses its right and left microphone to track down a low frequency emitter with a bandpass filter!

Likes : 1    Views : 157
Comparing Direction of Travel Methods ME461 UIUC

This project compares the ways of obtaining a compass angle, using the MPU-9250 gyroscope, MPU-9250 magnetometer, and motor encoders.

Likes : 1    Views : 157
Movin' and Groovin' SegBot (UIUC ME 461)

SegBot that dances to the beat of a song using a microphone and beat detection algorithm

Likes : 1    Views : 155
Adaptive Cruise Control based on RobotCar

The final project of ME 461 at the University of Illinois in Urbana-Champaign. My RobotCar is based on the TI F28379D Launchpad.

Likes : 1    Views : 153
EasyBreathe: Hardware + Firmware

We are the Hardware and Firmware team for EasyBreathe and we focus on the PCB and firmware development of the electronic mask.

Likes : 2    Views : 146
UIUC ME 461 Frequency Controlled Segbot

Using different frequencies, we can make the self-balancing segbot turn left and right as well as go forward.

Likes : 2    Views : 143
The Cookie Soldier - ME461

Ever wanted a robot to find cookies for you? Well now, that's possible. WARNING: Robot may develop cookie addiction

Likes : 1    Views : 141
UIUC ME461 Final Project

A demonstration of the use of PI feedback controller compared to an open loop controller. This project was done for ME461 at UIUC.

Likes : 1    Views : 140
Robot Pet Project

I designed and created a robot that follows me around and plays a variety of different songs when I tell it to.

Likes : 1    Views : 139
UIUC ME 461 Final Project

My final project is a sound following segbot that tracks and follows frequencies with a microphone and the TMS320F28379D LaunchPad.

Likes : 1    Views : 139
UIUC ME 461 Two-Wheeled Segbot with Microswitch Sensors

This two-wheeled robot uses gyroscopic and accelerometer information to balance, with two front sensors to sense when it has hit a wall.

Likes : 1    Views : 133
Coin sorting robot car

This project is a small car that will accept US coins, and automatically sort them based on denomination.

Likes : 1    Views : 132
Bluetooth Steering Segway Robot

This balancing "Segbot" receives commands wirelessly over Bluetooth that are interpreted as steering instructions (UIUC SE 423)

Likes : 1    Views : 130
BumpBot Clutter Counter

This bot self balances and travels through the room autonomously. It beeps the amount of times it has hit something

Likes : 1    Views : 129
UIUC ME 461 Final Project --Ryan Fogle

As a part of my ME 461 class, I used a TI board and an Orange PI Zero to wirelessly control the bot on two wheels through a website.

Likes : 1    Views : 129
Untitled Goose Project

A goose that will find you and chase you to the ends of the earth.

Likes : 2    Views : 119
Waltzing robot

Segbot that dances to music and recognizes different notes from a song and reacts to their notes.

Likes : 2    Views : 105
TI RSLK MAX Enhancement - Base Kit

Contains information on the base RSLK MAX kit as well as the IR sensors and gripper arm.

Likes : 2    Views : 105
WIFI Controlled Segbot

Segbot that balances with PID control and can be commanded to move through commands in Linux terminal.

Likes : 2    Views : 102