University

Hackster.io projects using Texas Instruments parts

Notice: The projects below are hosted by Hackster.io and posted by the Hackster community. By clicking on a project, you will be leaving Texas Instruments’ website.

LaunchPad Development Kit

Home
Adding Bluetooth Connectivity to DPS3005 Power Supply

I hacked to DPS3005 power supply, by connecting a TI CC2640R2F LaunchPad using UART interface to add Bluetooth connectivity!

Likes : 1    Views : 800
How to Create a CMSIS DSP Library Project for Hercules: FFT

A step-by-step guide to create a project with the Hercules CMSIS DSP library.

Likes : 3    Views : 798
Micromouse Autonomous Vehicle Kit

The Micromouse Autonomous Vehicle Kit is an all-in-one robotics set designed for the Micromouse competition and as a beginner learning kit.

Likes : 2    Views : 780
IoT-Based Socket Board

A portable socket board is designed that can be controlled through internet. It provides portable automation solution of devices with ease.

Likes : 7    Views : 778
Bluetooth Low Energy Power Bank

With a Bluetooth Low Energy Power Bank you can use a Smart Phone App to see how much charge it has and receive notifications if its charge.

Likes : 2    Views : 775
Hercules LaunchPad MkII: ePWM Example

Simple how-to guide to set up the ePWM module of your LaunchPad and increase / decrease the duty cycle with the two user buttons.

Likes : 3    Views : 768
Hercules TMS570LS04 I2C Driver Library

The Hercules TMS570LS04 does not have I2C hardware. We turn the onboard timer into an I2C master.

Likes : 1    Views : 766
Button Mashing Counter

Have your friends ever gotten mad and accused you for button mashing at Super Smash Bros? Well now your name is cleared!

Likes : 2    Views : 757
MSP432P401R Driver for Pixy2

This is a driver with user-friendly functions that provides interface between the Pixy2 and the MSP432P401R microcontroller.

Likes : 5    Views : 756
IoT-Based Robot with Temperature Notification System

We can send this robot to remote places where humans cannot reach, and can also get the temperature of that place.

Likes : 1    Views : 752
Motion Sensor Based Device Control

Optimize the energy consumption by activating your appliances only when human being are present in a room.

Likes : 7    Views : 737
Real-Time Device Control

Now automate your appliances smartly by setting the time when you want your gadget to switch on and off

Likes : 5    Views : 730
Smart Light Switch (UIUC - SE 423 - TI LaunchPad Project)

Google Assistant integration with openHAB on Orange Pi Zero, telling Texas Instruments MSP430G2553 Launchpad to drive servos on light switch

Likes : 2    Views : 726
Hitachi LCD Driver Example for the Hercules LaunchPad

Hitachi compatible LCDs are the most common char based displays. This project shows how to drive such a display from a Hercules LaunchPad.

Likes : 0    Views : 725
Finite State Machine on a MSP430

How to program a MSP430G2 Launchpad with Finite State Machines (FSM) using YAKINDU Statechart Tools in your Code Composer Studio.

Likes : 2    Views : 715
Mewzk Layzer

The highest quality sound in a small. lightweight package.

Likes : 1    Views : 715
A TEMPorary Solution

Wearing shirts and shorts, but it's 40 degrees outside? Wearing a hoodie and sweats, but it's 103? Never again with a TEMPorary Solution.

Likes : 4    Views : 711
Fly!

A mini-game where players fly a star among obstacles, provided for you.

Likes : 3    Views : 701
Hercules LaunchPad CAN Bus Test Gig

Poor man's CAN tester with 2 diodes and 1 resistor.

Likes : 1    Views : 698
Rocket Payload

In this project, we designed a rocket payload that measures altitude using the barometric pressure and temperature of the air.

Likes : 6    Views : 694
Rental Cycle

It is a rental cycle or a calories burner. we can rent it for particular duration and the amount will be deducted by users digital wallet

Likes : 10    Views : 693
Joy Pen

A joystick controlled pen capable of simple drawings with a MSP432 at its base. Final project for Applications of Embedded Systems.

Likes : 5    Views : 692
Hercules Driver Library for Hitachi LCD Displays

Driver library makes Hercules LaunchPads and Hercules micro controllers work with Hitachi type LCD.

Likes : 1    Views : 689
Synergia Theremin

Music doesn't get better than this. (With this LaunchPad and a piezo buzzer at least.)

Likes : 1    Views : 679